I would like to confirm LM26001 simulatuon by webench.
I cannot simulate in the below conditon;
- Vin: 16V < Vin < 38V
- Vout: 12V
- Iout: 1A
I tried it but I saw the comment;
- This design is not stable due phase margin......
- Circuit Calculator can't create design.
In the case of LM26003 and Iout = 2.5A, I could simulate it.
Why can I simulate it?
Best regards,
Atsushi Yamauchi