This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI buffer IC Maximum clock frequecy

Can SN74LVC3G07DCUR be used to buffer SPI lines?the load capacitance in my case will be 120pF?So can this IC be used for this purpose?

if this ic can be used to buffer spi lines,then what will be the maximum spi clock frequency that it can buffer?