Hi
I will request the IBIS-model of SN74LV161ANS.
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I will request the IBIS-model of SN74LV161ANS.
Best regards
IBIS models can be requested on the Web bench forum. However this part is 20 years old so there may not be data available to create an IBIS model.
Maximum operating Vcc is 5.5V. Anything beyond this, functionality is not guarranteed. The part will not be damaged with Vcc up to 7V but all limits and functionality will not be guarrenteed when operating beyond recomended operating conditions.
Hi
I would like to request an IBIS model.
Method of procedure?
Best regards
Please ignore the text of the following TPA.
It is the failure of Editer.
I will move you request to Web bench forum.
As I said this part is old enough to where there may not be data available to build IBIS model. We will see what they say.
Thanks for your inquiry.
As Chris stated, IBIS model is based on simulation of the design database which for this particular part is no longer available.
Lab measurement based model is another possibility but this requires product line’s support. Chris should be able to comment if that is a feasible option.
Regards,
-Eric Kim (WEBENCH Design Center)
If you want to request this then we need to continue this By email. I will need the business case to see if we can do it. c-cockrill@ti.com
Hi
I appreciate your support.
We would like.
Please ignore the following text. (TPAxxx......)
It is in the error of Editer.