This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150

Other Parts Discussed in Thread: LM3150

Hello,
I used Webench to create a schematic for the LM3150 DC-DC Converter.

Input: 26~32 V; output: 24 V /8 Ampere;
I have not changed the component types, manufacturer.
(1)I found the temperature of LM3150 is about 80°C.
Is the temperature high
when LM3150 works ?
(2)
The output voltage  drop below 24 V (about 15V).    

Is there any suggestion for this case?

  • Hi Vega,

    Are these results from simulation or from bench measurements?  If they are from bench measurements, can you please include the PCB layout file?  This may help us debug further.

    The maximum operating junction temperature for the device is 125degC, so 80degC may still be acceptable.