Hi,
I imported the file attached in TINA-TI software (version 9.3) and got the message "Successfully compiled". Then I tried to create a macro (Tools | New Macro Wizard) using AC_INPUT_PT.cir as the file in the "From file" input. After I selected "Auto generate shape" option, and pressed Next button, the following errors were shown:
1. "Undefined model: E.(C:\Program Files (x86)\DesignSoft\Tina 9 - TI\EXAMPLES\SPICE\TSPICE.LIB)"
2. "The circuit cannot be opened or cannot be converted to a macro."
Is there anything wrong with this file or I am doing something wrong?
Thanks,
Cícero.
)