I'm having difficulty getting a circuit model in TINA to work (3005.Deliyannis.TSC). The circuit is intended to be a simple test of a single supply modified deliyannis filter centered at 40kHz. It keeps saying VF1 has an unconnected pin which will be connected to ground & capacitor C4 has an unconnected pin which will be connected to ground, then the analysis popup shows an irregular circuit error. I recheck the ERC and the errors go away, but the analysis will not run.
Apologies for a question that probably gets asked too often, but I did try to search for the answer and the solutions did not seem to help in this case. Much thanks for any help!