Hi,
For the LP2989 regulators, I only see HSPICE models on the website. I want to simulate a design where we are using this regulator. Where can I grab the 3V version of this regulator for TINA-TI (if it even exists)?
Thanks,
Phil
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks, I wasn't sure if there was a specific simulation area to post in.
I can only find PSPICE models for the 3.3V version on the part description page and couldn't get it to import successfully into TINA-TI.
Hi Philip,
Please find attched the TINA test bench for LP2989-25.
The test bench is set up for the following condition:
Vin(min) = 2.81V, Vin(max) = 4.25V, Vout =2.5V, Iout = 0.2A , Optimiser position = 3V
webench_design_3847317_1686.TSC
Thanks,
Ajit