Hello,
I would like to know if it is possible to add a TPS2115 5V autoswitcher from TI to a Power architect design in Webench. Our design needs to switch between two 5V regulators and we would like to know if it is possible to incorporate additional TI components such as the TPS2115 in the webench power architect design. Below is our current design and the depiction of our desired change follows. Help with this question would be much appreciated.
Thanks