Hi,
I checked the output voltage of the LM2678 (no load connected) and it was 7.9V, when a load was added it lowered the Ouput voltage to 1.6V and the current output was also too weak, approx. 0.3A. Any suggestions?
Thanks and Regards
Andi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I checked the output voltage of the LM2678 (no load connected) and it was 7.9V, when a load was added it lowered the Ouput voltage to 1.6V and the current output was also too weak, approx. 0.3A. Any suggestions?
Thanks and Regards
Andi
Andi,
We need some more information to debug your issue. Please attach your simulation files so that we can look into this issue for you.
Thanks,
Hi,
I did not simulate the design, I only tested it.
It is impossible for me to attach the Layout in a public Forum, but in the table below you can find how the output changes depending on different inpunt parameters.
INPUT (Power Supply unit) | OUTPUT |
12V | 1,5V (0,3A) |
10V | 1,9V (0,4A) |
8V | 3V (0,9A) |
6V | 3.5V (1,5A) |
5V | 3,8V (2,1A) |
4V | 1,5V (0,7A) |
Thank you and Regards
Andi