Hello Team,
I have a customer who is interested in using the LM2678 for their upcoming designs. They are using the webench simulation tool to study the device. For their input parameters Vmin = 8V Vmax = 40V, Vout = 12V and Iout = 5A, there was no simulation generated. I tried with the same parameters and got the same result. However when I input 20-22V, Vout= 12V Iout = 5A, I do get a simulation. Is there an issue with webench for this device. How can the customer evaluate this device for the specs they need.
Thank you for you time and attention towards this issue.
Sincerely,
Kishen