Other Parts Discussed in Thread: LSF0101, , LSF0102
Tool/software: WEBENCH® Design Tools
lsf0108 ibis doss not allow selecting it as an output for hyperlynx simulation and lsf0101 and lsf0102 ibis models report errors when trying to assign them to simulation
I see the lack of output for the 108 has been asked before in the forum, but I do not see anyone following it up with a response
thanks
error for 102
C:\hyperlynx91\9.1HL\SDD_HOME\hyperlynx64\Libs\lsf0102.ibs:
Warning : at line 82 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Only the first combination from the [Series Switch Groups] will be used.
Warning : at line 123 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Only the first combination from the [Series Switch Groups] will be used.
Error : at line 4109 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 4 to pin 5 of component LSF0102DCU does not exist in this file.
Error : at line 4109 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 3 to pin 6 of component LSF0102DCU does not exist in this file.
Error : at line 4109 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 4 to pin 5 of component LSF0102DCT does not exist in this file.
Error : at line 4109 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 3 to pin 6 of component LSF0102DCT does not exist in this file.
Error : Parse failed on file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0102.ibs.
error for 101
C:\hyperlynx91\9.1HL\SDD_HOME\hyperlynx64\Libs\lsf0101.ibs:
Warning : at line 82 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0101.ibs : Only the first combination from the [Series Switch Groups] will be used.
Error : at line 4067 in file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0101.ibs : Pin model LSF0101_IO_S used by the series pin mapping from pin 3 to pin 4 of component LSF0101 does not exist in this file.
not output option for 108
Error : Parse failed on file C:/hyperlynx91/9.1HL/SDD_HOME/hyperlynx64/Libs/lsf0101.ibs.