Other Parts Discussed in Thread: TINA-TI, ,
Tool/software: TINA-TI or Spice Models
I downloaded the TPS22918 TINA SPICE model from your website. I put TPS22918_TRANS.LIB, TPS22918_TRANS.TLD AND TPS22918-Q1_TRANS.TSM into C:\Program FIles (x86)\Designsoft\Tina 9 - TI\SPICELIB directory. When I start up the TINA program is says "New Library Detected: Library must be recompiled. It may take a few minutes. Continue?". I click yes. Program starts, I click on 'tools, find component' and type in TPS22918, then click on search. It shows the part in the SPICE macro window. I then click on 'insert'. It then gives a message about the macro not being present in the library and asks to be rebuilt. I click 'yes' but it seems to ignore it since it comes back with the same question. Now everytime I restart TINA it comes back with the original message about a new library was detected. Appears to be a vicious software circle that I can't get out of. Is there another file that I need - or do I need to put the present TPS22918 files into another directory?