Part Number: BQ25504EVM-674
Tool/software: TINA-TI or Spice Models
Good morning,
we contact you for a problem with the simulation of the BQ25504 EVM on PSpice.
The output voltage is not regulated from an input voltage over 1 Volt. The component have in output a voltage value higher than the Over_Voltage, with the same value of resistances and capacitors of the commercial EVM. In a real simulation I see the output voltage ever limited on 4.2V, but software simulation purpose an output voltage higher then 5 volts.
Have you an idea when the problem is?
Regards,
Contini Stefano