Other Parts Discussed in Thread: TINA-TI, OPA330,
Tool/software: TINA-TI or Spice Models
Hi Everyone,
I have been trying to get used to using TINA, which is a great simulation software when it does work, but I just seem can't get it to work.
For example the schematic shown below, when I add in the instrumentation amplifier circuit, OPA330 for some reason stops working.
If I remove INA333, then it works again. I have encountered the same issue in the past, it seems to me that TINA has problem simulation more than one IC?
Simulation with both INA333 and OPA330, as shown by the graph, Vout which is the output from OPA330 is at 1.65 flat, when I should see a sine
wave with 200mVpp biased at 1.65V.
VG2 = sine at 100Hz with 200mVpp and biased at 1.65.
Simulation without INA333 circuit, as shown in the graph, once INA333 has been removed, OPA330 simulates correctly.
VG2 = sine at 100Hz with 200mVpp and biased at 1.65.
I have not changed the OPA330 circuity at all, I only removed the INA333 circuity.
Is there a reason why this is happening?
The reason for the OPA330 circuit is because I was using it to remove the DC offset from the INA333, however it wasn't wokring and after some debugging I found
that the opamp just wasn't doing anything. Please see this post https://e2e.ti.com/support/amplifiers/precision_amplifiers/f/14/t/633065.
Thanks for the help.
Rgs,
Bryan
I have included the schematic from TINA here.