This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS55165-Q1
Tool/software: TINA-TI or Spice Models
I am trying to simulate TPS55165-Q1 in fixed 12V output in pspice, when I try to connect BST1/BST2 to cap as recommended in the datasheet, I get an error saying the pin is floating , I have tried running in multiple machines but the issue remains same, Please see the screenshot below,
SETUP:
Error:
N03722 is the node name for the wire connected to BST1, N03726 is for BST2.
When I try to connect it without cap, it works fine till 3ms and output travel back in time at 12V constant. i.e., out is 12V like I want but in time 3ms-0ms,which shouldn’t be possible. I have attached project files fyr.
TPS55165-Q1_sim.zipslvmca3a.zip
In reply to Abhishek Tripathy:
Hello Abhishek,
I appreciate you response. I have used SPB 16.6 ( cadence 16.6) to draw the circuit, I tried simulating without using caps at those pins, I would get 12V at 1.2ms but from there I observe output in reverse direction.
I have attached the waveform fyr.
I have used the same file to simulate the below response
Circuit:
Waveform:
even when I connect BST1 and BST2 directly I get the same response
Regards,
SAINATH D
In reply to Sainath d:
I have attached the cadence 16.6 files again.lm55165-Q1.zip
Hi Sainath,
I simulated the project shared by you. It runs absolutely fine. Please find results below.
I feel that there is some issue with loading the large data file in AMS simulator on your system.
I hope this clarifies your query.
Thanks & Regards,
Abhisek