Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hello every one,
I'm try to use the BQ25504 as Booster and energy harvester, so actually, i set the Vov=5.4 V and Vuv=2.7 V, so this is OK.
So the problem is about VBAT_OK, it set it to 3 volts (with the values of the datasheet), as result i have a VBAT_OK to 5.4 volts (like Vstor).
so can you help me to understand where is the problem please.
Rov2=6.53M / Rov1=3.47M
Ruv2=5.37M/ Ruv1=4.63M
Rok1=4.42M / Rok2=4.22M / Rok3=1.43M
I did the tests on the EVMBQ25504 evaluaiton board.