Tool/software: TINA-TI or Spice Models
Hi
I need a simple functional model for some logic functions - D type flip flop, XOR gate and a time delay (I need to be able to set delays from 100ns to 5us .
It would be nice too, if there was a square wave generator with a settable duty cycle (about 0.5%) - I'm using a Pattern Generator for that at present, it works but it's a bit of a kludge.
I haven't seen anything in the TINA libraries so is there a way I can implement these functions. I'm not worried about rise times, fall times and so on, just simple 1s and 0s will do nicely.
Thanks
Colin