SwitcherPro Desktop 3.17.0.0 Crashing under Windows XP SP3
The error message I get: http://pastebin.com/HiS8BpWG
I tried running the application as administrator and it doesn't help.
We will investigate and get back.
Ahmet,
We tried to do a fresh install of SwitcherPro desktop version on Windows XP SP3. It worked fine. Please find the details of my machine below.
Do you already have an older version installed or is this a fresh install? I would recommend you to do a fresh install and this time don’t pick the first option "Yes, migrate my designs". Please let us know if this helps.
Thanks,
--Abhi
Hello Abhi,
Thanks for the answer.
I did a fresh install with the same version you did, and did not pick the option "Yes, migrate my designs". However, this didn't help at all. I still have the problem.
Would it be possible for you to send us the 'SwitcherProDT.evt' log file. Here are the steps on how this can be done:
Also, please send us the information of your OS using the following steps:
Is there a way you can use the web version in the mean time?
Thanks & Regards,
Thanks for sending us the OS details. One thing that I noticed is, you are using Turkish version of OS. That could possibly be a problem. However, I would still need SwitcherProDT event log to be able to investigate this in detail.
Is it possibly for you to use online version in the mean time (as an alternative)?
-Abhi
The file you have requested is in the attachment.2158.Log File.txt
Thanks Ahmet.
We will investigate into this issue and get back to you.
Regards,
Hi Ahmet,
We were able to reproduce this issue. The problem is installing SwitcherPro on Windows XP SP3 with Turkish regional language settings. Unfortunately at this point we do not plan to fix this. However you can do one of the following.
1) Use SwitcherPro online version.
2) Install SwitcherPro Desktop on Windows XP SP3 with US-en language settings.
Dear Abhi
thanks for your reply and i use already in web.
regards.