Use the SwitcherPro design software to create a TPS5410 VinMin: 10.000 VinMax: 32.000 Vout: 3.300 Iout: 0.800 and C9 on the input side is automatically set to a 10V ceramic capacitor when the VinMax is set to 32V.
The SwitcherPro design software needs to put in at least a 32V capable capacitor. If I actually built this circuit, it would crackle and burn.
Any ideas?
This bug has been fixed in our tool but it's not pushed out to the production web site yet. It should be updated very soon. I agree this is a really bad bug. It looks like the Input caps were being selected against the worst case output voltage rather than the worst case input voltage.
this is fixed in production now.