• Resolved

WEBENCH® Tools/LM5022: change the value

Part Number: LM5022

Tool/software: WEBENCH® Design Tools

Hi Team,

I did the structure of a boost on webench, and i found the result below,

Vin: 8 V
Vout :  125 V / 0.2 A
on the result i found the value equal 33uH, i want to increase this value. What is the max value that i can put it??
and
 if i change this value, what i need to change other value of the components ?
Best regards