hi,
I was made a simulation and a desing of a booster with Vin: 5-8 V output 12V 1A, but my circuit not working (don`t have errors about the desing with webench because i have all components (Except the mosfet because i have the NTD4963N)).
The Pin 1 have a signal with high frequecy, but with amplitude of 250 mv Aprox.
Vout is the same with Vin.
I dont have signal in base of transistor (NTD4963N).
DIS*/EN is not connected.
Can you help me please??5102.webench_design_3679925_13_488606997.pdf