Using a 10 to 50V input range with 0.016mA output and 4V with the TPS54062 use to give the following result:
with a 1mH inductor. it now gives:
with a 3.3mH.
I was wondering if someone could help by explaining why there is a difference, and which one is better.
Thanks for the help
Philip