I would like to use an LM3409HV to drive a single CREE MT-G2. Vf=36V, Iled=350mA, Vin,min=46V, Vin,max=50V. The LM3409HV is a bit over qualified for the design, but we stock it and it has excellent dimming capability.
Unfortunately I cannot get Webench to create a solution. The LM3409HV is in the exclusion list, with a comment of "Circuit Calculator can't create design".
Is there a way to get around this to see a potential design?
I can use the Excel calculator, but I would really like to use Webench as a check.
Thanks.