1)Why LM5085, can not be used (according to the Webanch)for:
Vin=45-57
Vout=6V
Iout=6A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM5085 should work in this case. Webench must have an error.
webench has lots of limitations that reject designs for various corner cases. I'll move this to the webench forum.
Hi Eli,
WEBENCH® could not create an LM5085 design because it could not recommend a FET based on the calculations with the design inputs. The calculated temperature of the FET exceeds the max temperature (which includes a safety margin buffer).
It may be still possible to create this design, but WEBENCH is not recommending a solution at these input and output conditions because it did not pass this temperature check for the FETs.