Is it possible to change capacitors in WEBENCH, and then see how it affects the circuit?
I know I can click components and choose an alternative, but I want to change it to something that isn't listed in the alternatives. That is, I'm designing a low-pass filter for 4.2KHz using Sallen Key, and the second stage shows C2 as 27nF. The closest cap I actually have in the lab is 22nF, and I want to know how if I can use it or not. The only alternatives in the list are all 27nF.
Thanks