Hi,
I have found that running identical sample circuits through Webench and Quickstart yield significantly different results.
I have been exploring both the LM21215 and LM21212-1 quickstart excel spreadsheets and Webench. The 2 spreadsheets are consistent with each other but, as I say, not with Webench. It also appears that Webench has problems with Vout less than 1.0 volts and with some values of the form Vout = 1.xxV
And, two problems just with Webench are:
a) it has no real save capability, so you can't be sure that it will remember how you had the circuit entered before
b) when going through various iterations of settings in Webench, it never remembers custom parts. If you DO manage to save a given circuit (how this happens is not clear) then it will remember the custom part. But, if you tinker with the circuit and it recalculates, then all previous custom settings are lost. This it REALLY LAME!!
Does anyone have any answers about the quickstart and webench models? Which is better/safer to use? I have to say, quickstart is easier and won't throw parts away, but maybe webench has better models? I don't know....
I have attached pdfs from both programs.
national_lm21212-1_0.9V_12A.pdfwebench_esim_426461_105_600035995.pdf