Hi,
This is an urgent request. I want to use LM5088 for Vin = 9 ~ 16V -> 5V and test it over 0.1 ~ 7A.
The initial parameters make me select an Io max = 7A.
In the simulation tab, the tool allows me to select Rload between 10 ~ 0.5 ohm which translates to a current range of 0.5 ~ 10A, when I run for Bode plot.
On the other hand, the tool allows me to select between 0.01 ~ 10A when I run for Load transient plots.
The datasheet doesn't really specify any minimum current range. Naturally, my components will be sized for Io = 7A.
I want to know how the circuit will perform for a 7A ~ 0.1A transient and vice versa as well as the bode plots for both.
Thanks!