Hi,
I am looking to design following switcher/boost circuit/DC-DC booster with following specs:
input: 3v3
output voltage:40v
output current: less than 1mA is okay The current is typically around 1uA
I am getting error when using calculated duty cycle exceeded limit. Any idea how to fix/design such circuit? My design parameters are obviously weird, but these are for very specific and real parameters in certain application.