When using the simulation tool (webench), I could not simulation only up to 10.1A. For that reason,Customer had a question. Why will the current be limited that low? the device is rated for 12 A and that is the input limit in webench as well. The current limit maximum in the datasheet is 14 A.
Why is the design not created?