Tool/software: WEBENCH® Design Tools
Hello
I am looking into ultrasonic flow measurement, and encountered a possible error on your Ultrasonic EVM / Transducer Selector.
When trying co calculate TOF in the TI Ultrasonic EVM / Transducer Selector at: https://webench.ti.com/webench5/TDC/index.html?app=flowHead i suspect that the equations use the wrong cos() function.
If I am to calculate the TOF with 45 degree placement I have to use the cos() in Radians and not Degrees to get the same result as the GUI. con(45)=sqrt(2)/2 = 0.707 and not cos(45)=0.525. A 46 degree angle would then give a negative delta TOF. As far as i can understand the cos() should be in degrees to work correctly. Is it correct that the error is within the GUI (the Ultrasonic EVM / Transducer Selector ), and you have implemented the wrong cos() function. Or is my calculations wrong?
regards Jarle Horneland