Other Parts Discussed in Thread: LM5166
Tool/software: WEBENCH® Design Tools
Hi,
My customer is using WEBENCH at LM5166.
We have a issue at Thermal simulation.
Please see "LM5166DRCT_22uH tab" and "LM5166DRCT_10uH tab" in the attached file.
Setting of WEBENCH at the first is Vin:24V, Vout:3.3V and Iout:120mA.
Then, inductance is changed from default value.
Customer selected two inductance which are 10uH and 22uH.
At using thermal simulation, customer has a issue.
Operation point of simulation result is same.
But the pictures of thermal have difference.
Could you let me know why we see this simulation result, please?
Best regards,
Shimizu