Tool/software: WEBENCH® Design Tools
Hi,
Does WEBENCH take into account the effect of DC bias voltage in MLCC's capacitance?
I mean, I have an application in which WEBENCH suggested a 10uF 100V as input capacitance. The input voltage is set to be from 30V to 40V. Looking at the suggested capacitor's datasheet, I found that when the DC voltage is 40V, the original capacitance drops to 50% (5uF). The same effect wil happen to all other MLCC on the circuit.
Does WEBENCH cope with this situation?
Thank you,
Yuri