Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Does the LM5060 model properly handle the OVP function?
In the attached simulation, which is the eval simulation file slightly modified, there is an OVP event. After the OVP event the output (OUT) goes to -10V, along with the gate (GATE). That doesn't seem right.
It's dependent on the load. In the attached simulation I have a 100 ohm load. A 1K load goes even further negative, and 10 ohm load goes only slightly negative.
I don't have an eval board, so I'm wondering if the model is accurately showing how the part functions.snvma08-overvoltage.tsc