Other Parts Discussed in Thread: TPS54334, TPS54334EVM-722
Tool/software: WEBENCH® Design Tools
I simulated TPS54335A's Webench on below condition, but failure and indicate "Calculated duty cycle exceeds limit" .
I think that TPS54335A Webench data have a bug because I tried Low fsw condition but same results, please confirm it.
If it was bug, please let me know about revision schedule.
・Vin: 13.2V~21V
・Vout: 12V
・Iout: 1.1A
【Additional information】
・When fsw is changed low value (100kHz, 500kHz, etc), results was the same (duty cycle exceeds limit).
・TPS54335A datasheet is described "Min off time: 0%"
・TPS54334 was simulate normally, I feel that TPS54334 and TPS54335A are near specification.
Best regards,
Satoshi