Other Parts Discussed in Thread: LM5122, LM5022, TPS40210, LM5022-Q1, TPS40210-Q1
Tool/software: WEBENCH® Design Tools
dear Sir
I can't use LM5121 to simulate below SPEC ,could you help to confirm ??
Vin=46V~50V to Vout=52V/4.8A
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kai,
We are currently looking into this issue with the LM5121. We will get back to you shortly.
You can try the inputs (46V to 50V Vin, 52V Vout, 4.8A Iout) in WEBENCH and I get the following products (LM5022, LM5022-Q1, TPS40210, TPS40210-Q1) in the solution list.
You could use them if they would meet your requirement.
Regards,
Gerold