Tool/software: WEBENCH® Design Tools
Hi,
Could you tell me about inductor selection criteria of webench?
The simulation results of webench became a following.
Recommended inductor was 1.2uH.
WebenchReportsServlet TPS53515.pdf
Customer input condition is:
-Vin:14V
-Vout:1.1V
-Iout:10.7A
-Fsw: 400kHz
However,It was 0.71uH when calculated based on the datasheet page24 ''Choose the Inductor''.
Please tell me the reason why the recommended value differs between webench and datasheet.
Best Regards,
Yusuke/Japan Disty