Tool/software: WEBENCH® Design Tools
Hi,
I am having difficulty in constructing a power tree for one of my project using Webench [pwer architect tool.
In the design, I have a primary voltage source of 5.4V DC. I am using a switcher, say PS1 to down-convert this to 3.3V/1.2A. Further, I need to add an LDO, say PS2 to derive 2.5V/0.15A from the 3.3V of PS1 supply.
But when I select option 'ADD LOAD', the LDO(PS2) gets added to the primary voltage source instead of the switcher(PS1) which is not intended. My requirement has multiple levels of voltage derivation from more than 1 switcher/LDO. Does webench has this feature?
Thanks