Tool/software: WEBENCH® Design Tools
Hi Webench Team,
First off I wanted to say that I love the tool and I'm blown away at all the incredible features and functionality that is included for free!!
I was using Webench to analyze the total system footprint of the LMR23610 and noticed the area for the ic seems a bit strange. In the footprint column on the BOM tab says "57" for the IC, however, there are no units here. Also looking at the datasheet I can only come up with a total area of 31(5 X 6.2)mm. Can you all please shed some light on why these 2 numbers are different.
Here is my design link: https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=790EFA679D08AA6F