Tool/software: WEBENCH® Design Tools
Hi all,
I have a problem with Allegro SPB 17.2 and Webench Connector for Allegro Toolbar (from now on Webench Toolbar). After i succesfully installed it yesterday (thanks Pradeep and TI for ultra fast support), it changed all my toolbar settings. So i positioned them again.
After i close Orcad and re open it it for a moment they are at the same position but after the script capAutoLoad_Webench.tcl runs, my toolbars became like default again.
So as you can see, it is very frustrating to fix all the toolbars each time i reopen Orcad. I even tried to hide Webech Toolbar, but when it starts again it reopens again. I saw the tcl script and thought if i could change it in order to show the Webench menu but not the toolbar, but it looks very weird like it is encrypted or something. Is there a fix to that?
Also, I think that it is worth mentioning that earlier versions of SPB 17.2 had that problem but it was fixed because when i first installed SPB 17.2 a few months ago and up until yesterday ( before I installed Webench Connector for Allegro) I didn't have that problem. Also if i remove the tcl script it works ok but then i cannot see trhe WEBENCH menu nor the toolbar, so there is no point in that.
Thank you,
Theocharis Vavouris