Tool/software: WEBENCH® Design Tools
hello,
I am currently working on a voltage regulation circuit that can handle approx. 24VDC at 10A.
The webench design is using the LM5176PWPR but none are available, is the LM5176PWPT the same pinout as far as the schematic below?
some other questions:
1) Does the LM5176 need an external oscillator to function, or does it have an internal crystal oscillator.
2) Based on the webench design, is this schematic ready to be prototyped physically? All of the webench simulations seemed great.
3) Novice question: What do the circled symbols in the attached figure below mean?
## attached below is the figure and the webench design link
Thank You,
Zach