Tool/software: WEBENCH® Design Tools
Hi
We tried to design an 500W, 500 kHz, Half bridge LLC dc-dc converter using webench. ( Input - 290 ~390 V DC, o/p - 19V @ )
I'm also attaching the Transformer design document from webench. It shows a Secondary winding RMS current of 53.7 A for which
a 31 AWG of 27 strands is given for secondary winding. A 31 AWG can carry around 0.4 A, how could 27 strands
of such 31 AWG could carry 53.7 A... Pls clarify.
And also the core size given is an EE25, even this 32AWG of 27 strands could not be terminated in those bobbins...
Thanks
Lenin.