Other Parts Discussed in Thread: LM5175
Tool/software: WEBENCH® Design Tools
I am curious about using the LM25085 outside the output current range that is specified in the WEBBENCH "Customize" options. As far as I can see, there is no reason that IC couldn't be used for an even larger load than 10A, so I would like to use the designer to investigate. I haven't found a tool that is so comprehensive and fast -- especially with the new redesign!
How are the range limits for each WEBENCH design enforced (specified by TI?), and is it possible to adjust them, perhaps on a temporary/per-user level? Or run a local version? Maybe there's a workaround already. Or I'm missing something in the datasheet and 10A is an appropriate limit.