Other Parts Discussed in Thread: LM1085, TLV62585
Tool/software: WEBENCH® Design Tools
Hi all!!
I'm trying design a regulator using the TPS7A7300 and I'm having problems in WEBENCH. The input voltage is 5V (USB), Vout is 3.7V and Iout max is 2.5A. When I enter this values in WEBENCH the result is an error, "Junction temperature is too high". I tried use the values showed in datasheet (Vin = 1.425 to 6V, Vout=1.25V and Iout=3A) and WEBENCH result an error too. Are there bugs in WEENCH or in TPS7A7300 model?