This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] DLPDLCR2000EVM: Links to BeagleBone Black Drivers for DLP® LightCrafter™ Display 2000 EVM

Genius 12860 points

Replies: 1

Views: 5884

Part Number: DLPC2607

Tool/software: Linux

Hello E2E Users,

If you are looking for the latest BeagleBone Black Drivers for use with DLP® LightCrafter™ Display 2000 EVM, please refer to the Debian release below:

https://debian.beagleboard.org/images/rcn-ee.net/rootfs/bb.org/testing/2017-08-01/lxqt-4gb/

> BBB-blank-debian-8.9-lxqt-4gb-armhf-2017-08-01-4gb.img
This image will always write to the eMMC flash on the BBB and install the Debian OS onto it. You are supposed to boot the system once with the SD card inside, then remove the SD card and boot without the SD card every time afterwards.

> bone-debian-8.9-lxqt-4gb-armhf-2017-08-01-4gb.img
This image boots directly to the operating system and runs off of the SD card. System files are saved to the SD card instead of the eMMC flash. You need to have the SD card inserted every time you boot with this image.

After downloading and installing the provided Debian distro to your BeagleBone Black, please refer to the DLP® LightCrafter™ Display 2000 EVM for more information on interfacing between your BeagleBone Black and the EVM.

We have received customer feedback that newer distributions of Debian (Stretch, 9.1) have had issues with loading this EVM's drivers. Until the root cause of this is identified, we recommend using the latest version of Debian confirmed to work with our EVM (Jessie, 8.9).

Best Regards,

Philippe Dollo

1 Reply

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.