This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DLP3000: No Connections

Prodigy 20 points

Replies: 3

Views: 156

Part Number: DLP3000

We were trying to connect DLP3000 system with our computer after installing DLPlightCreatev1.1 software in the gui window it seems we are unable to connect to the system. 

In the network connections we are seeing unidentified network. We followed each and every step in your manual guide very dilligently 

  • Sourajit,

    Welcome to the E2E forums, and thanks for your interest in our DLP technology.

    I'd like to ask you for additional details on your issue so we can assist you further. What operating system are you running. In addition, what do you mean by "unidentified network" in your system configuration settings? Finally, which system are you trying to connect via GUI? Is it the LIGHTCRAFTER EVM (using the DLP3000 DMD) featured here?:
    www.ti.com/.../DLPLIGHTCRAFTER

    Thanks for your input.

    Best Regards,
    Philippe Dollo
  • Hello Sourajit,

    What operating system are you using? Are you trying to connect to the Lightcrafter EVM or is it your own system? Could you also please try using the latest GUI which is version 5.0.0 and can be found at www.ti.com/.../DLPLIGHTCRAFTER (date is 2013).

    Thanks,
    Kyle
  • In reply to Kyle Rakos:

    Hi Sourajit,
    Were you able to resolve the issue after updating to v5.0.0 package? We haven't heard from you, i am tentatively closing the issue, feel free to get back to us, if we can help you further debugging the issue.
    Regards,
    Sanjeev

    If a post answers your question, please click on "Verify Answer" button

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.