This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/DLPC410: RST_ACTIVE is not asserted regularly

Intellectual 265 points

Replies: 26

Views: 1300

Part Number: DLPC410

Tool/software: Code Composer Studio

Hi,

Our setup is as followed: (Virtex7, DLPC410, DLP7000)

https://e2e.ti.com/support/dlp/f/94/p/759718/2806469

As we have resolved the previous problem, the DLPC410's initialization and calibration go successfully, and we can also retrieve the right DMD_TYPE and VERSION. However, the control outputs somehow couldn't get to the mirror, and I'll list some of our observation below:

1. The RST_ACTIVE stays low even after we output BLK_MD = 11, BLK_AD = 1000, ROW_MD = 00, ROW_AD = 'd0, and other control signals (e.g. wdt_ena, rst2blkz, ns_flip ...) weren't toggled during the output.

2. ECP2_M_TP16 (Clock reset) stays high after initialization. We're not sure if this is normal and what causes this if it is not.

Thanks,

Justin

  • Expert 4310 points

    In reply to Justin Chen14:

    Hi Justin,

    May I know which version of DLPC410 you are using and what dmd_type and version is read? In latest version ECP2_M_TP16(version 7) is expected to be high.

    All the Block mode and block address information will be ignored unless there are valid row cycles taking place. DCLK should continuosly be provided to the DLPC410 and a valid row cycle is when DVALID is asserted for an entire row. If there are no clocks nor DVALID assertion, then no DMD reset will occur.
    There are PLL differences between Virtex 5 and Virtex 7.
    Please double check dclks using oscilloscope.

    -ykc
  • In reply to ykc:

    Hi,

    DMD_TYPE:0001, VERSION: 5

    When the PLL and LVSD modules are ready, the DCLK will always be provided. And after the initialization, our DVALID is constantly logic high (we checked the LVDS output using oscilloscope).

    This is our DCLK measurement, is this a valid one?

    In addition, we want to know what is the mechanism of ECP2_M_TP5 (DVALID_A) assertion. Does it indicate directly our DVALID LVDS signal from APP_FPGA, or is it an indication of the validity of the DVALID + DATA  signals? If it is the latter one, and if we measured those signals using an oscilloscope, how can we know if they are valid or not?

    Thanks,

    Justin

  • Expert 4310 points

    In reply to Justin Chen14:

    Hi Justin,

    Dvalid latches the block and mode settings and indicates start of row operation when it is asserted. It should be deasserted after 16 clocks
    Please check Figure 8. DLP7000 / DLP7000UV 2XLVDS DMD Input Data Bus.

    When you say Dvalid is constantly high. You mean right after initialization it stays high?
    Please try keeping it low, adding some delay after init then assert it.

    Please also check Figure 3 of datasheet regarding timing requirements of these signals.

    -ykc

  • Expert 4310 points

    In reply to ykc:

    Hi Justin,

    DCLK scopeshot you attached is it differential signal ?

    -ykc
  • In reply to ykc:

    Hi,

    " It should be deasserted after 16 clocks"

    How long should it be deasserted? We now deasserted it for 2 clocks after asserting it for 16 clocks but the TP5 is still not asserted.

    "Please try keeping it low, adding some delay after init then assert it."

    We now keep it low after init and then assert it.

    "Please also check Figure 3 of datasheet regarding timing requirements of these signals."

    Both of our NS_FLIP and COMP_DATA are constantly logic low.

    "DCLK scopeshot you attached is it differential signal ?"

    We found that the LVDS clock gets well after we inserted a GBUF for the reset pin of the LVDS module. This is our DCLK signal now.

    Thanks,

    Justin

  • Expert 4310 points

    In reply to Justin Chen14:

    Hi Justin,

    Clock certainly look better now. For now keep delay to 32 clocks. Please check skew requirements of Skew, BLK_MD, BLK_AD, ROWMD or ROWAD to DCLKIN in section 8.5.

    -ykc
  • In reply to ykc:

    Hi,

    We found that when we deasserted the ARSTZ, the INIT_ACTIVE will only be asserted for 14ms, unlike the 220ms assertion on the datasheet.

    What could possibly cause this, and will this cause any other problem such as the lack of training pattern lasting time?

    Thanks,

    Justin

  • In reply to ykc:

    And please we would like to know the mechanism of the ECP2_M_TP5 assertion.

    Thanks a lot,
    Justin

  • Expert 4310 points

    In reply to Justin Chen14:

    Hi Justin,

    When you deassert ARSTZ, training pattern is applied beforehand ?

    In Xilinx FPGAs (due to the construction of the ISERDES and OSERDES cells) a pattern
    of 0010 needs to be applied to the output/transmitting SERDES cells data pins (D1 = 0,
    D2 = 0, D3 = 1, D4 = 0) in order to receive a result of 0100 (Q1 = 0, Q2 = 1, Q3 = 0, Q4 =
    0) at the input/receiving SERDES cell.
    The patterns should be applied on all of the input data and DVALID pins. In this respect,
    the interface is treated as a 17 bit interface with DVALID being the 17th data bit. The
    receiving logic in the DLPC410 will shift the data until the correct pattern is seen at the
    inputs. The SERDES cells align the incoming data with the ½ speed system clock (derived
    from the full speed data clock). This allows DLPC410 to correctly align the DVALID signal
    and the incoming data and will contribute to a more robust interface. It is important that the
    training pattern is applied to the DVALID and data inputs of the DLPC410 before reset to
    the device is deasserted, as training commences immediately on the deassertion of reset.
    The INIT_ACTIVE signal is asserted while the device is held in reset in order to help
    facilitate this behavior.

    After initialization is
    complete, a delay of at least 64 DCLKIN clocks (on all input data buses being used) should be observed before
    the first DVALID is asserted on those data buses to ensure a clean start up process.

    -ykc
  • Expert 4310 points

    In reply to ykc:

    I checked the D4100 kit which has Virtex 5 and I can see init active asserting for 237ms. After this atleast 64 clks delay is needed.
    During training patterns no signal should be applied on row, block pins.

    -ykc

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.