This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DLPC3438: Write Image Crop/Write Display Size/Write Display Image Orientation could not work

Prodigy 30 points

Replies: 2

Views: 133

Part Number: DLPC3438

Hello:

     Board info :  dlpc3438+dlpa2000+dmd

     Use the specified read command, i get the Controller-Device-ID is 0x05, DMD-Device-ID is 0x60 0x0D 0x00 0x87.

     This system already works, the DMD generate the correct screen in test Pattern.(Color bars, Horizontal lines, etc)

      I can correctly control the Test-Pattern-Select to show different images, and control the LED Current to make image more brightly.

      But when i need to set the image display size, or make image Orientation, it does not work!

 

      For example, I want to sent the display size to : 1280 * 360

      My control Command as this: x_dlpc_wr 2 0x12 4 0x00 0x05 0x68 0x01

Op.Cmd DLPC.No Op.Code(Write Display Size) Length Byte1 Byte2 Byte3 Byte4
x_dlpc_wr 2 0x12 4 0x00 0x05 0x68 0x01

     And, of course, I tried a bunch of configuration parameters, no one works, And i don't know why.

     

      I guess there are some reasons for this problem:

1> My Config parameters is error. (This is unlikely to go wrong, Because some of the configuration items are already working correctly)

2> The firmware(Boot Code) on the external flash have some weakness.

3> May be some hardware error,etc

Please help me solve this problem.

Thanks a lot,Best wishes!

  • Hi Jianmin,

    This command is of 8 bytes.

    I noticed in our Programmer guide it is mentioned 4 byte.

    Thanks for raising this ticket, we will fix our programmer guide.

    Use command parameters : 00 00 00 00 00 05 68 01

    Thanks,
    Navneet
  • In reply to Navneet Singh:

    Hi Navneet,

    It works correctly use 8 Bytes command, Thanks very much.

    Thanks, best wishes!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.