This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DLPA3000: Can I use PWR6 of DPLA3000 to power focus motor?

Intellectual 360 points

Replies: 12

Views: 626

Part Number: DLPA3000

Hi, Sir

Currently, we have a DLP driver board (DLPA3000+DLPC3438), I want to use PWR6 as the power supply of motor driver chip (A3901). So it's possible or not?

Thanks

Br

Tao

Tao

  • In reply to Azad:

    Hi, Azad

    Thanks, acutally, we have another host to control Proj_on to DPLC3438. So I thinks I can provide 3.3V by DPLA3000, right?

    Thanks.

    Zhang Tao

    Tao

  • Expert 5275 points

    In reply to Zhang Tao:

    Hi Zhang,

    Yes, as long as the load current doesn't exceed 200mA.

    Regards
    Azad

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.