This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DLPDLCR3010EVM(not G2) :Can't use DLP LightCrafter GUI

Expert 1415 points

Replies: 14

Views: 568

Hi.

I can't use DLPDLCR3010EVM(not G2). (TIDA-00384)

This message is displayed on GUI Window.

--------------------------------------------------------------------------

Command " _DeviceArrivedCommand" : Bad expression;

WriteGPIO(0x220,0x220)

WriteGPIO: failed

---------------------------------------------------------------------------

What will I solve if I do it?

I tried with some PCs and I think that EVM is a problem.

Regards,

Rei

  • Expert 4495 points
    Hi Rei,

    Can you explain when this error occured? Did you get this error on starting the GUI or after a specific action?

    Regards
    Azad
  • Expert 1415 points

    In reply to Azad:

    Hi Azad,
    Thank you for your reply.

    The message displayed starting the GUI and pushing Get button.

    I think Cypress USB-Serial Configuration Utility option is wrong.
    How do I set it up?(SCB0,SCB1-I2C,SPI?)

    Regards,
    Rei
  • Expert 4495 points

    In reply to rei:

    Hi Rei,

    Are you able to read your EVM's Cypress chip configuration using the Cypress USB-Serial Configuration Utility? If so, can you share your current settings?

    Regards
    Azad
  • Expert 1415 points

    In reply to Azad:

    Hi Azad,

    Thank you for your reply.

    Regards,

    Rei

  • Expert 1415 points

    In reply to rei:

    Hi Azad,

    Would you please provide your comment?


    Regards,
    Rei
  • Expert 4495 points

    In reply to rei:

    Hi Rei,

    Please find below the configuration:

    Regards

    Azad

  • Expert 1415 points

    In reply to Azad:

    Hi Azad,

    Thank you for your reply.

    I set the same configuration.

    But the same error occurred.

    Connect the EVM to USB:

    Push the "Get" button:

    Projector and switches are working .

    I think that firmware is no problem.

    Regards,

    Rei

  • Expert 4495 points

    In reply to rei:

    Hi Rei,

    Can you confirm that you're using the DLPLCRD-GUI v7.0? If so, please try the DLPDLC-GUI and see if you're getting the same error.

    Regards
    Azad
  • Expert 1415 points

    In reply to Azad:

    Hi Azad,

    I used DLP LightCrafter Display v7.0.

    I installed DLPDLC-GUI.

    Push the 'Get" button.

    Error message:

    Get EVM Information Error!

    Error while trying to gain access to the I2C bus.

    Regards,

    Rei

  • Expert 4495 points

    In reply to rei:

    Hi Rei,

    Did you reflash the MSP430 on the EVM or is it running the factory default code?

    The Cypress bridge must be the I2C master in order for the GUIs to work. It's possible that the MSP430 is not relinquishing control of the bus, which could be why you're getting these errors.

    Can you trying reflashing the MSP430 on the EVM with the reference code available here: www.ti.com/.../DLPDLCR2010EVM

    Regards
    Azad

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.