This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/DLPNIRNANOEVM: TIVA source code compilation

Prodigy 70 points

Replies: 12

Views: 689

Part Number: DLPNIRNANOEVM

Tool/software: Code Composer Studio

Hi everyone,

I'm trying to compile the Tiva Source Code from the NIRscan Nano, but I'm getting two errors:

Description Resource Path Location Type
#20 identifier "calibCoeffs" is undefined cmdDict.c /Mobile Spectroscopy TIVA EVM/App line 75 C/C++ Problem
#20 identifier "scanConfig" is undefined cmdDict.c /Mobile Spectroscopy TIVA EVM/App line 64 C/C++ Problem

I follow the steps from B and C section of the DLP NIRscan Nano EVM (Rev. G)  but I can't build the project.

 I'm using CCS V6.1 and the other versions of the build are shown below.

Thanks.

12 Replies

  • Hi Guillermo,

    Could you try switching form CCS 6.1 to 6.0.1? Also please confirm you are using TI-RTOS 2.10.1.38 and TI ARM Compiler 5.2.4.

    Thanks,
    Kyle
  • In reply to Kyle Rakos:

    Hello!

    I'm using TI-RTOS 2.10.1.38 and I've switched to CCS 6.0.1, but I coudn't find TI ARM Compiler 5.2.4 nowhere (I'm using 5.2.9 instead). I'm getting the same two errors.

    The version of NIRscanNanoSoftware is 2.1.0 and the DLPSpectrumLibrary is 2.0.3.

  • In reply to Kyle Rakos:

    Ok, I've found how to dowload TI ARM Compiler 5.2.4, but I get the same two errors.
  • In reply to Kyle Rakos:

    I got the same errors, any solution?
  • In reply to Guillermo Rego:

    Hi Guillermo,

    Kindly wait for a few days, we'll get back to you regarding this soon. Thanks for your patience.

    Thanks & Regards,
    Hirak.
  • In reply to Guillermo Rego:

    Hi Guillermo,

    Could you kindly let us know your OS version? Kindly Also try using CCS v8.1.0 for building.

    Thanks & Regards,
    Hirak.
  • In reply to Hirak Biswas:

    Hi,

    I'm using Windows 10 Home x64. With the v8.1.0 I get the same error.

    Regards.

  • In reply to Guillermo Rego:

    Hi Guillermo,

    Have you added the dlpspeclib as a dependency to the MOBILE SPECTROSCOPY TIVA EVM? Kindly double check that dlpspeclib,usblib and driverlib are all added as dependency to the MOBILE SPECTROSCOPY TIVA EVM project.

    Thanks & Regards,
    Hirak.
  • In reply to Hirak Biswas:

    Hi,

    Yes, I added all the dependencies. I followed all the steps shown in the DLP® NIRscan™ Nano EVM User's Guide (Rev. G). I tried also in a Windows 7 OS.

    Regards.

  • In reply to Hirak Biswas:

    Hello,

    any news about this?

    Regards.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.